This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS732-Q1: capacitor recommendations

Part Number: TPS732-Q1


Hello,

I am using the TPS732-Q1 to generate a precision reference. My end equipment has a lot of high powered motors and is polluted with EMI. I am using the adjustable version of TPS732-Q1 to convert 5.5V to 5V @ 150mA. Given that it is on the border of VIN-VOUT=0.5V, can you recommend -

1. Output cap value

2. A cfb value that I can start with the rationale behind it

Thanks,

Rohit Joshi