I have 6 pieces TPS62130 on my board. Sometimes one of them does not work when I enter 12V input pwer. But sometimes it works. This is a random event which affects stability. I need to improve it. Since it does not work when I enter 12V input pwer, I need to shut down 12V and wait for more than 25 seconds, and then enter 12V again, it may rework to generating proper output voltage.
Here are the schematic and layout.
Here are the signals in the 12V-TO-5V unit when it works well.
Yellow is Vin and EN, 12V, light blue is SS / TR, dark blue is 5V Vout.
Here are the signals in the 12V-TO-5V unit when it does not work.
Any help would be much appreciated as this is the only thing holding up production and it is urgent!
Besides, when I use the DC electronic load machine to test one unit of tps62130 on my board, it works well up to 3A current in the CR mode even if I turn on and off 12Vin repeatedly. However, in the CC mode above 1.6A current, it only generating about 200mv. The SW signal is below. what is the state of work?