Hi,
I need an accurate 2.85VDC with low current, 20mA. I need 2% minimum accuracy. Am I better off using the TPS799285DRVR fixed output or should I use an adjustable such as the TPS79901DRVR? Which one will be more accurate assuming I were to use 1% resistors for the adjustable? If I use 0.1% does that make the adjustable more accurate?