Part Number: TPS60150
Hi
My Customer has question.
The customer says it can not be adopted unless the contents of the question clear.
Please give priority to this question and respond.
1.In the data sheet of TPS60150, Co min = 2.2 uF is stated.
This effective capacitance includes any DC bias effects?
2.If it falls below 2.2 uF, is there a possibility that the TPS 60150 malfunctions?
For example, "output oscillation" and "breakage" etc.
Capacitor the customer is about to implement may not satisfy 2.2 μF due to its characteristics.
customer is concerned that it will lead to "oscillation" and "breakage".
※Please especially please give priority to 1 and 2.
3.The customer use it with Vin = 3.3 / Vout = 5 V/, but there is a possibility that the Vin may become 0 V.
At that time, Vin = 0 V / Vout ? 5 V/Load=Open.
Does TPS60150 get damaged?
4.Is there no problem even if I operate the TPS60150 in a state where the output has a voltage (Pre-Bias)?
Best Regard