Tool/software: WEBENCH® Design Tools
Hello,
my customer have problem with power unit in his project,
the circuit contain two power units:
1. the circuit no.1 - input 32 volt, output 24v 5A (he checked the 24v and found it o.k but no current test yet)
2. the circuit no.2 - input 24 volt from circuit no.1, output is 5 volt 0.5A.
circuit no 2 doesn't work at all although it show in WEBENCH that it should work fine.
I would be glad if you can advise me back if you have alternative solution with the same pinout it will be great as well, thank you.
Regards,
Shai Berman