Other Parts Discussed in Thread: LM5021-Q1, , LM5022-Q1, TIDA-01344, LM5022
Hi, my customer is designing on board charger and need to choose a flyback controller.
The requirement is:
1. automotive qualified
2. current control mode, CCM mode, maximum duty cycle>50%
3. internal slope compensation, output overcurrent protection.
4. output power>150W.
Besides the four requirement above, it's better if PSR can also be met.
After searching our products, I recommended LM5021-Q1 to the customer which can meet their requirement, the only disadvantage is PSR is not met.
The customer is also interested in UCC28630, which can meet all requirement including PSR, the only problem is that it's not automotive qualified.
So my question is:
do we have the plan for UCC28630-Q1 part? If yes, what's the schedule?
If not, do we have any other devices that can meet all the requirement and will be automotive qualified by the end of June 2018?