Other Parts Discussed in Thread: LM5117,
Hello,
do you have some sample solution or app no that you would like to deal with adding programable current control for LM514 or any similar non isolated DC-DC controller?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks you for information.
I'm going back to the LM5145
It is worth trying this or it will be very unstable
Big red 1 is standard CV control loop with internal error amplifier
Big red 2 . Measure current on low side shunt amplifi this voltahe on curr. Amplifier and this voltage compare with Vref for required max current in CC mode. Output of this fast comparator is for example 0V or 3V. This voltage goes over diode and Rc to CV FB.
If output current is under set current is on output CC comp 0V and all works in CV mode. if output current exceeds set max current is on output CC comp 3V which are dividers on resistor divider Rc/Rfb2 on voltage higher than 800mV. Because on FB is overvoltage LM5145 redice votage and thereby reduce current.
Does it have a chance to work or will it be a very unstable solution?
I am very sorry, I edited my initial response because I misunderstood the app note you were referring to. I believe the basic implementation will work, you will need to make sure the current loop is slower than the voltage loop.
Hope this helps?
David.