This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM36922H: Full-scale ILED Setting under Enabling via PWM

Part Number: LM36922H

Dear, Sir.

My customer is considering to apply LM36922H as bach-light driver for Smart Phone.

They don't want to use I2C interface" because their system only has PWM signal.

The other side, they are expecting the dimming ratio over 511 steps.

Currently, ILED is set on 25mA by the external resistor for each strings.

Please give your advice as following to propose the best product for them.

1.  I would like to confirm the Full-scale ILED Setting(100% duty) under Enabling

    via PWM.

    Is it set on 25mA separately on each 2 strings?

2. I suppose LM36922H will be better to realize the higher dimming ration.

    Please introduce the best product if there was something alse.

Best Regards,

H. Sakai