We are revisiting a project working with the UCC28950 designed for 2KW output power, 390V input, 200-360V output and a switching frequency of 100kHz. As we began working with our transformer manufacturer for some prototypes there has been some concerns raised about the transformer requirements generated by the calculation spreadsheet. Specifically, the primary RMS current and the Primary Magnetizing Inductance. The calculator using the above data at the 200V output requires around 1.8mH magnetizing inductance and 16.5A RMS current. The manufacturer is indicating that a transformer to meet these requirements would be significantly larger than most transformer we have seen in this power range as well as it being gapped at nearly 3cm. Are we missing something here?
Thanks
Mark