Other Parts Discussed in Thread: BQ25890, BQ25895, TPS2514A, TPS2546
Can I use the BQ25890H in OTG mode as a charging device? For example 5V 1,5A.
Is it possible to short-circuit the conclusions of D + and D- with BQ25890H?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for the answer.
I want to enable bq25890h by this scheme:
At the ID signal, I will recognize which type of device I connect to the USB. If the ID is floating, then SDP / DCP / CDP is connected to the USB. If the ID is connected to GND, then I want to include a boost mode and apply for 5V VBUS voltage and current up to 1.5 A, ie be a charger (Dedicated Charging Port). The question is, can bq25890h short-circuit D + and D- to be defined as DCP?
Sorry for the bad english.
Hello Sergey,
Yes, you can short the D+/D- lines to force the bq25890H to detect DCP always for input current limit when in charge mode. You can short them or use a 200Ohms in between the lines.
When in OTG mode, you would configure the boost mode output in REG0A which lets you set the OTG current limit and the output voltage. Closest current limit for your requirements would be 1.4A.
The device connected to the USB port expecting to see a DCP would need to see the correct D+/D- termination (in this case a short).