Hi,
On the datasheet 7.3.5, minimum load is required as follows;
"A minimum load of about 5 mA is required to fully recharge the boot-strap capacitor in the minimum off-time."
Does the minimum load value depend on another condition(i.e. VIN, VOUT, fsw, etc...) ?
I would like to know if minimum load about 5mA is allowed on the below condition.
VIN=12V, VOUT=3.3V, fsw=500kHz
Best Regards,
Kuramochi