Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, EV2400
Hi ,
I am not getting battery information from fuel gauge. I have configured the fuel gauge from below parameter. is any correction required to configure the gauge?
is any extra work or parameter is need to get the battery information?
/*
//1st-class ID,2nd-offset,3rd-data,4th-length
{48, 12, 1400 ,2}, /* Design Capacity = 1400mAh */
{48, 14, 5180,2}, /* Design Energy = 3.7 * Design Capacity */
{48, 00, 3700 ,2}, /* Design voltage = 1400mAh */
{34,00,4200,2}, /*charging voltage*/
{80, 64, 3600, 2}, /*terminate voltage */
{2 , 5, 3600, 2}, /* UV Prot Threshold 3600 mV */
{2 , 8, 3700, 2}, /* UV Prot Recovery 3700 Mv */
{2 , 0, 4200, 2}, /* OV Prot Threshold 4200 mV */
{2 , 3, 4100, 2}, /* OV Prot Recovery 4100 Mv */
{36 , 0, 100, 2}, /* Taper current */
{36 , 4, 4200, 2} /* Taper voltage */
*/
Thanks,
Bhavna Harani