Good Day. Apologies in advance for asking about such a venerable part. It is still in current production in lots of packages, though, so there is demand and field use of the part.
Some documentation refers to protection circuits which may be added to the feedback pin (COMP INPUT) to stop noise on that pin from interrupting the inductor charge cycle by driving the pin above the 1.2x V reference level momentarily. This contradicts the description and normal operating plots in which a full charge cycle is completed even after the feedback pin voltage is higher than the reference in the same documents. Was this a legacy problem from the TL497 which made its way into the documents for the TL497A?
More important to current actions, referring to document SLVA143, "Designing Switching Voltage Regulators With TL497A":
Does the TL497A ignore changes in feedback pin status during a charge cycle as shown in Fig. 4?
or
Does a momentary high voltage on the FB pin momentarily interrupt the timing capacitor charge process as shown in Fig. 14(b)?
Thank you in advance.
Andrew