I have questions about TPS54550.
Question 1.
Pleaase tell us the maximum value of capacitor at SSENA pin.
Question 2.
If we connect the resistor at SSENA pin, how it works the slow-start time?
Best regards,
Takahiro Nishizawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Nishizawa-san,
The plot in figure 21 is just a graph of equation 3 on p. 8 of the datasheet. That was done 12 years ago, so I do not remember all the details, but so far as I can recall SS was not tested over that entire range. Theoretically, you should be able to extend the slow start time even beyond 80 msec, but most users have SS times in the range 0f 1 to 20 msec, so I use that as a general rule of thumb. I haven't seen any issues with those times unless there is an over current condition or there is a large amount of output capacitance. Slow start causes the output voltage to ramp up at a linear rate. You are also charging the output capacitor bank. the charge current required is I = C * dV / dt = Cout * Vout / tss. If the required current is larger than the current limit. The TPS54550 will eneter hiccup mode and continuously restart.
ss time is the time for Css to charge from 0 V to to 0.891 V. The SS cap will start to charge when both Vin is above the UVLO and EN is asserted. Please bear in mind that the tolerance on the SS charge current is quite wide, 1.8 uA min, 5 uA typ, 10 uA max.
Nishizawa-san,
I have not been able to get the simulation to run for the first case yet. It will not complete without hanging up. Now I am engaged in a customer emergency. It is very likely I will not complete it this week. I'll keep you posted if I have any progress.
Nishizawa-san,
I have measured the EVM SS time. Enclosed please find the results with some analysis.