Hi,
Please review the attached LM3481 Auxillary power supply design.
I have never worked SEPIC converter before ,so kindly check the schematic and give me review comments as earliest.
Following are my design specifications:
I/P Voltage: 21V-30V
O/P Voltage :24V
Current: 2A
Note:I have followed Ti webench power designer ,According to that design have created
- In current schematic from webench there is coupled inductor 150UH which is big foot print ,kindly suggest me this inductor can be replaced by small inductance value.
- I have gone through several design application note,based on that design calculation ,inductance value coming arround 12UH coupled inductor.
- In webench switching frequency is 554KHZ.
- so im considering 554KHZ for inductance calculation.(Duty cycle is 54%).
- Auxillary power supply design for TI review.pdf Also while considering duty cycle which duty cycle need to consider minimum or maximum duty? becoz if your considering minimum duty cycle maximum input voltage has to consider for calculation
and suppose if your considering maximum dutycycle need to consider minimum input voltage. so give me some information on this .
- At output side i have considered one electrolytic capacitor .need another two capacitor?