This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: wrong output and device overheating

Part Number: LM27761

Hello. I am having problems with LM26671 regulator. I have input 5V, and want to generate -2V output with current draw of about 1mA.

I have the schematic and layout here.

What I am seeing is, after powering out, I would have output at -2V for some time, and then the output would go to 30 mV (VFB 10-20mV), and I can feel from the bottom of the board, the component is overheating.

What is the problem here?

Thanks very much.

I am attaching