Hi,
In the following forum post it was suggested to change the Flash Update Ok Cell to 999mV for a NiMH.battery: https://e2e.ti.com/support/power_management/battery_management/f/180/p/491414/1794498
This is a large discrepancy from the default 2800mVolt. In a setup with a 10s1p NiMH-battery where the chemical ID incidentally was the same, 6100, we could calculate from the formula given in the datasheet upon calibration of the voltage Divider value: Flash Update Ok Cell = 800m*10*5000/17583 = 2275mV. However, with these values Update Status and Max Error don't change as expected during the learning cycle. When setting Flash Update Ok Cell to 999mV, however, it appears to work.
Two questions:
1. The voltage divider value after calibration is 17583 as compared to the calculated 15740. Is this difference prohibitively large?
2. With Flash Update Ok Cell at only 999mV what will be the minimum voltage for a flash update?
Thanks in advance,
Gustaf