Other Parts Discussed in Thread: TPS40170, TPS28225-Q1
What is driving the 20A max limit posted on the TPS40170 product page? Looking to use this chip for 25~30A and the only thing that seems to me to limit the max output current (of a synchronous buck converter to be clear) is the ILIM pin which is largely driven by RDSon of the low side FET. It seems to me if you select a low side fet with low enough RDSon that it should not be an issue. Does the MFR recommend use for loads above 20A? Any limitations?