This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24232H: junction temperature

Guru 29720 points
Part Number: BQ24232H

Hi Team,

I would like to estimate Tj (junction temperature) under the following condition.
---------------------------
Vin = 5V
Vbat = 3.0V
Ichg = 0.2A *No system load
Ta = 25 deg
---------------------------

I calculated as the following in desk theory.
Is it correct?
-----------------------------------------
P1= (Vin - Vbat) * Ichg = (5V - 3.0V) * 0.2A = 0.4W
Tj = Ta + (P1 * θJA) = 25 + 17.8 = 42.8 deg
-----------------------------------------

Best Regards,
Yaita / Japan disty