This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030: LMR14030

Part Number: LMR14030
Other Parts Discussed in Thread: TPS254900-Q1, LM25141, LMR33620

Dear Sir,

My customer looking for a replacement part for LMR14030 with similar specs but higher efficiency.

The target is to have this buck converter operating at 95% or above efficiency under 12V Vin, 5V Vout, 1.5A Iout conditions.

Any type of buck converter is fine.

This part has to be able to co-work with TPS254900-Q1 USB port controller.

Could you help suggest suitable parts?

Thanks, Ian.