This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS22933 data sheet, page 3, Absolute Maximum ratings, sec. 6.1 Table:
There is no absolute maximum voltage specified for pin CAP, pin 6. Please advise maximum value of voltage and/or current on pin CAP.
Thanks,
John
Hi JCC,
CAP is an output, so there are no max voltage or current ratings for this pin. If a voltage or current is applied, then there will likely be damage on the pin.
In general though, the highest voltage on this pin will be the highest input voltage used. In the case of this device, this can be 12V.
Thanks,
Alek Kaknevicius