This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have prepared to add a PWM ramp and offset circuit to CSA and CSB as shown below. Before enable the PFC, we find the waveform at D2105 is look like ch2 waveform as shown below (Fig.1 single trigger). Is it normal waveform? Do you have the correct waveform to share with us? Thanks.
Fig.1
Fig.2
Hello Derek,
Your waveforms were not attached to your posting but I will try to explain what you should expect with the help of SLUA479B application report.
The ramp and offset adds a small DC error signal to the CSA and CSB signals. This is shown above as the "false current sense signal".
It is just a DC voltage that stops gate drive that would otherwise would result due to an erroneous current transformer signal.
Therefore you should be just adding a small DC signal to the current sense resistors.
REgards
John
Hi Derek,
The compensating waveform that you should expect to see is a small dc offset with a ramp on top.
I think that is what you have.
You should run your pfc circuit so that you get the proper signals from the current transformers. Then perhaps add your DC offse and finally add the ramp.
Check the effect of this compensating network.
A lot of users will just used the small DC offset.
This will create a small dead zone around the zero crossings of the AC waveform where there is no PWM switching
Regards
John
Hi John,
Will the dead zone around the zero crossing you mentioned will affect the power factor or not? If yes, how to improve the power factor. What I have done is we add the compensation circuit and found the power factor is lower than before. The circuit is in the attached file. Please help.
Hello Derek,
I can think of no reason for doing this but you should try the experiment and check the results.
Regards
John