Other Parts Discussed in Thread: BQSTUDIO
Hi Onyx
I'm having trouble creating a GMSF file in BqStudio for the BQ27220 (using EVM2400). I'm always getting "Reading the data memory or flash image has failed The golden image files could not be created".
Additional information:
- EVM2400
- bqStudio 1.3.52.1 (also tested with 1.3.86)
- When this happens, the "Progress Information Image Files" window says "Reading data memory: Address 0x9180".
- Maybe related: When go to "Data Memory" > "Read All" > "Write All" (without changing any default value) I get a red error message on the bottom "Value is beyond minimum value defined for parameter.:Calibration.Current.CC Gain"
- I can reproduce this just by starting up, going to Golden Image and then hitting "Create Image Files"
- OTFS files are created without problem
Thanks for your help!
Best,
Mark