Hi,
Another question for BQ24079. The datasheet specify the OUT pin voltage regulation Vo(REG) is 5.5V. But we see 4.3V at output when a battery is installed and the device powered by USB. Without battery installed, the output is 5V, which is same as Vin. So, what voltage should I expect from OUT pin when battery is installed?
Thanks,