Hello Team,
according to the data sheet the max current into Vsense-Pin is specified with 1.5uA at Vsense = 5V. This is valid for TPS3702CX50, correct?
Question:
Will the Vsense current be proportional to Vsense voltage or will is stay constant for the different versions (TPS3702CX12, TPS3702CX18, TPS3702CX33)
In other words: Is the resistance of the 3 resisistors the same for all versions or does it change with the version?
If the current stays at 1.5µA for all variants at Vsense = 5V will TPS3702CX12 Isense,max be proportional lower: Isense(max) = 0.36uA @ 1.2V?
Is the sum of all 3 resisitors constant over all variants?
Thanks and Best Regards,
Hans