This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear ti,
I have read the slua585 design resources,there is a description of a paragraph in the below
I see the bq24610 spec the Vrch typical:50mv,I setting the Iterm=0.3A, so the Rbat_max=50mv/0.3A=166.7mΩ,
Is there right?
thanks®ards
None
None,
Good day.
Yes, your calculation is correct. So you should make sure your resistance between charger output and battery terminal should be lower than 166.7mohm.
Otherwise you will see BQ24610 will charge and terminate repeatedly during battery absent situation.
Thanks
Hi Paul Yeh
if my battery output resistance Ro≤300mΩ,that it means to i should change my Iterm so the Iterm max≤50mv/300mΩ=0.167A,at the bq24610 spec demand to Iterm≥0.125A,so in my design,the Iterm should set to the range [0.125A,0.167A].
is there right?
Thanks®ards.