Dear ti,
I have read the slua585 design resources,there is a description of a paragraph in the below:
BAT Output Capacitor or Resistance is Out of Range
For host control charger, a data sheet will give a recommended inductor and capacitor value base on the
LC resonant range.
For stand-alone charger, it not only has a LC resonant range, but also has Cmax_wake or Cmax_dis
calculation which is derived from the battery detection parameter [see bq24610 data sheet (SLUS892)]. If
the output capacitor is over Cmax, the status pin will flash even when battery is absent.
Also, if the resistance is too high between charger output and battery terminal, the charger will run in and
out of charger termination.
Rbat_max = Vrch/Iterm
Vrch: Recharge threshold voltage; mV/Cell
Iterm: Termination current.
Rbat_max is the resistance between charger output and battery termina?
Rbat_max is the internal resistance of cell?
Rbat_max is The sum of the two ?
Looking forward to your reply.
Thank you.!