This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
I am trying to use the BQ24610, but it seems that there is no function to know the gas gauge.
Are there any ICs that include a gas gauge in addition to the BQ24610 function?
*Adapter 24V , bettery 5cell
Hello,
I would recommend implementing the charger and gauge separately. If you are looking at a 3-4S pack then the bq40z50 would be the best choice with included protections. If you are looking for 5-6S then the bq40z80 would be the best choice gas gauge. If you only want gas gauging and no protections/cell balancing then you can look into the bq34z100-g1.
Sincerely,
Wyatt Keller