Other Parts Discussed in Thread: CSD18531Q5A
Hi,
The schematic diagram of the circuit being debugged is as follows.
The relevant parameters are as follows.
(1) Input voltage : 24V;
(2) Battery charge voltage : 12.6V;
(3) Battery charge current : 2.8A;
(4)Precharge and termination current : 0.3A;
(5)Safety timer: 9.3h (CTTC-0.1uF);
Charging function is normal, but the chip bq24610 temperature is very high. The surface temperature of the inductor is also very high. Heat sink pad is connected to GND, and copper coating area is also large.
Please help to analyze the possible reasons.
p.s. Input voltage is 15V, the temperature is not high.