Other Parts Discussed in Thread: LM3478
Hello team,
One of my customer use LM3478 to generate +-40V from 12V battery, the output voltage of P_40V_NEG_ISO became unstable ( fluctuate between -37.5V and -39.8V, no rule) and P_40V_POS_ISO is stable. This issue happens when the temp of LM3478 rise, the load is a 1.5Kohm resistor in the output.
Could you help check below schematics and give some feedback?
For the R340, could you let me know the function of this resistor? Can we remove it? Thanks.
Dongbao