This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are using the TLV70215 and looking at the output capacitor ESR requirements.
The datasheet states the equivalent ESR should be less than 200mOhm.
We have a 10V, 1uF Multi-Layer Ceramic Capacitors (MLCC) on the output as well as a few local 100nF bypass caps around our FPGA.
<< ESR across frequency image copied below >>
At what frequency range should we evaluate ESR from the datasheet curve?
This curve shows greater than 6 Ohms at DC & 0.7 ohms at 7MHz.
The 100nF bypass caps and they have similar ESR curves. Even if we consider them all to be in parallel, we have around 2 Ohms of effective ESR on the output caps of the regulator at DC.
Could you please let us know if this is a problem?
If so, could you recommend an output capacitor that would be better?
Thank you, Keith