This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are two questions about uc1846 as following:
1, Regarding the duty cycle adjust.
We can see the Figure 10 open loop test circuit on page 11 in spec of uc1846 in which the duty cycle can be adjusted via changing the voltage of pin5. but in fact, the duty cycle could not be adjusted when changing the voltage of pin5, I have no idea why ,please tell me the reason?
2.Regarding dead time adjust. when adding external PWM signal on SYNC (PIN10) and the CT (connect to between Pin8 and ground) will be shorted. So,
how much is the dead time ? Could Istill adjust the dead time?
Hi Joe,
Sorry for the late reply.
Thanks for your supports! I got the duty cycle.
Regarding to the dead time , we know the deadtime is set by capacitor Ct . My question is how much the deadtime is if using extral sync signal to control the PWM output based on the Ct is grounded ?
Thanks,
John
Hi John,
In this case I suspect that the dead time will be set by the width of the Synch signal applied.
In normal operation the dead time is set by the time taken for the internal 12mA current source to discharge CT. Hence the dead time can be adjusted by varying the value of CT. This discharge period will also define the width of the synch pulse output on Pin 10.
When CT is grounded the oscillator is effectively replaced by the external Synch signal applied to Pin 10. In this case the width of the Synch pulse should define the dead time.
I hope this answers your question.
Joe Leisten