Dear colleague/friends.
I have some questions by using BQ24350 device. Now my customer needs a over voltage protection device. VIN: 12V to 26V ( not battery input, DCDC power supply ), and ovp occurs when vin>30V , now they are using LTC4365 device, adjustable OVP/UVP threshold by external resistors.
I just find it seems TI do not have adjustable UVP/OVP threshold device( by external resistors ). But I find BQ24350 series device, below are my questions,
1. How could we set OVP threshold value? For example, when VIN>28V, OVP occurs. OUTPUT voltage is 0V. Or it is set internally?
2. what does below Input over-voltage protection mean?
3. What is the role of BAT pin? OVP threshold set pin?
Thanks very much.