Hi,
Does this chip can read the battery voltage ?
I have went through the datasheet but couldn't figure it out.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does this chip can read the battery voltage ?
I have went through the datasheet but couldn't figure it out.
Joice,
The TPS65721 itself does not read the battery voltage. The PMIC has a single comparator for low battery voltage, set by VBAT[1..0] in Register 05h and the default value is 2.2V (00b). At this point, the battery is completely dead.
There is also a VLOWV parameter (3.0V typical), and if the battery voltage is between 2.2V < VBAT < 3.0V then the PMIC will perform the following actions:
"If the BAT voltage falls below VLOWV during the battery detection test, it indicates that the battery has been removed. The device then checks for battery insertion. The FET Q2 is turned on and sources IPRECHG out of BAT for the duration of tDET. If the battery voltage does not rise above VRCH, it indicates that a battery has been inserted, and a new charge cycle begins. If the voltage rises above VRCH, it is possible that a fully charged battery has been inserted. To check for this, IBAT(DET) is pulled from the battery for tDET. If the voltage falls below VLOWV, a battery is not present. The device continuously checks for the presence of a battery."
This may be the root cause of the current draw you are seeing.
The TPS657201 & TPS657202 have an Internal Analog Multiplexer (BAT, TS, TS_OUT) for the processor to read the battery voltage from an ADC, but the TPS65721 does not offer the multiplexer (MUX).
Joice,
A few comments here:
First of all, there are 3 IRMASKx registers (IRMASK0, IRMASK1, IRMASK2) and I would like to make sure that IRMASK0 and IRMASK1 both read back 0xFF. Assuming they both read back 0xFF and IRMASK2 is set to 0xFD, then you should only be getting an interrupt driven by the PB_STAT (push-button status change) event.
Secondly, you mentioned you used a 180k pull-up to 3.3V on INTz. The TPS65721EVM-516 uses a 100k pull-up from the INTz pin to LDO1. Where is your 3.3V rail generated and why did you choose such a weak pull-up resistor? The current should be low for GPIOs, but maybe it is too low and the pull-up is not working as expected. Generally speaking, this would mean you have a non-zero voltage on the INTz pin. If you measure INTz and see a voltage between 0.4V and 1.8V, this could mean the pull-up resistor is just too weak.
Finally, you are testing the interrupt from the push-button, but you did not say how the PB_IN pin is wired and I do not see any schematics you shared previously. I cannot simply assumed you have the PB_IN pin wired correctly. Although this may sound trivial, please verify PB_IN is pulled up to VSYS through a 100k resistor and is pulled to GND through a physical push-button (when the push-button is pressed, PB_IN is shorted to GND directly).
If none of these suggestions work, you will need to share you schematic, scope shots of the issue occurring, and a data log of I2C transactions to the TPS65721 device. A "register dump", or reading all registers and sending them as a .CSV file can also be helpful.