Hello TI,
We have question about TPS92692. Is there has something errors can cause it not switch? thanks.
Currently we check the pin voltage level of tps92692, as below:
VIN 24VDC, VLED 36V / 150mA, OPEN analog to pwm dimming, fPWM 250Hz
IADJ 1.2V
DIM 1.2V
VREF 5V
VCC 7V
FAULT 7V