Other Parts Discussed in Thread: BQ500215, BQ501210, BQ51013B, BQ51021
Dear technical support,
I recently started working as an R&D engineer and my first job is to debug a board containing the BQ51025 the former engineer made.
The problem comes when i have started to try the board and while it works fine connecting with the transmitter it starts to limit itself to 540 mA.
I have tried adding potentiometers in Rfod (0-1000 ohm) and in Rlim (0-2000 ohm), calculating all possible solutions and getting a regression of the current that should be flowing thought the load, It works fine between 300-550 mA but when i ask the board for more power(lowering resistor load from 20 ohm to 10 ohm at 5 V) it starts to limit power.
Later I had another potentiometer added in the voltage feedback circuit to be able to change the voltage and therefore finding out where the limit was, with this i am able to set the circuit in the full voltage range(0-8V roughly), and then i found that i am not able to go up of 5.5V (550 mA ) with a 10 ohm load even if Rfod is (200 ohm) and Rlim is only 100 ohm(by my calculations that should be 1.5A limit.
Also I have disabled all power limiting and FOD systems in the emitter and is connected to a power supply so it should be delivering 5 watts but i'm only getting 2.7 Watts at best.
Any idea of why this can be happening?,