This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is using TPS65910 as the PMIC of the AM3354. But they have some questions about the startup waveform.
As you could see below waveform, VPLL have the Startup overshoot, same as VDAC, VMMC, VAUX2.
Besides, for the VDD-CORE, it has weird ladder waveform as below.
Could you please help to provide some advice for this? Thanks.
Hi Biser,
Sorry that I've made typo, which should be Am3354.
Could you please help to check the startup waveform?
Thanks.
Hi Biser,
There is one more questions about the VDD-CORE waveform. As you can see the below picture, the VDD-CORE has a step down voltage while the system is running. Does this has something to do with the Linux core frequency?
By the way, while testing the pin of the TPS65910: SCL_SDA_SDI, the waveform has the 400mV dropout? Could you please help to provide some advices?
Thanks.
Hi Ahmad,
Do you mean these step down waveform is okay? Could you please help to provide more details about the changing voltage on VDD_CORE?
By the way, while testing the pin of the TPS65910: SCL_SDA_SDI, the waveform has the 400mV dropout? Could you please help to provide some advices? There is 4.7kohm pull up resistor to VAUX2.
Waveform as below:
Hi James, I don't have any advice regarding the 400mV drop-out. Does the VAUX2 source have the same drop-out?
Regarding voltage changes on the MPU and Core: git.ti.com/.../board.c