Hi,
I have a bq27510 EVM and an MSP430 microcontroller connected via I2C. I have succesfully communicated to the gauge and have read values such as control status, flags, temperature, voltage, etc.
On the other side, I have generated a DFI file for the cells I'm planning to use using the appropriate app note (slua449d)
Right now, I'm trying to write the DFI file via I2C. I have already managed to upload the data to the microcontroller, so now I have to reproduce the flowcharts on figures 8, 9 and 10 of slua449d.
The thing is, this flowcharts are a rather large sequence of undocummented commands for erasing and writing the data flash (this is called "ROM mode" in the datasheet). I'd like to know if is there any other tool to help code and debug the DFI write process, such as:
- Code samples
- Explanations of what do these commands mean, or what outcome should be expected of them
- Sequence of command types to generate a read the golden pack info stored in the gauge. this might be a intermediate step and also could give final verification of uploaded data
Any of these would be really appreciated.
Thanks in advance!
Jose