Other Parts Discussed in Thread: TPS23751, , TIDA-00617
Hello,
I am using the TPS23751 to power my design. I already produced a couple of 100 boards and sometimes I see weird behaviour of the output voltage. During startup some of the boards starts oscillating a bit. The oscillation is between +-200mV around the original voltage. I also see this kind of oscillation when I attach a heavy load(2Ohm) and then just disconnect it. Is this reliable to my first problem?
P.S. I don't see this behaviour at all the boards.