Dear TI members
I am reviewing the schematic of my co-worker but have some question related to TPS40170
Q1) Input voltage : 12~24[V] , output voltage : 12[V]
I think that there is a problem when the input voltage is apply to 12[V].
Is that correct ?
Q2) My co-worker said to me " TPS40170 can output 12V/20A(output).
is that correct?
Because i didn't find out the output power/current from specification , I want to know that Output current with output voltage.
Input Voltage :24V , Output Voltage Setting : 12V Output Current : ?
Thanks