Dear TI ‘s engineer,
there is a customer ask for a question about that how much is the temperature of UA78M12C thermal overload protection? from the datasheet just show the device has internal thermal overload protection,and the operating virtual junction temperature is 150℃,if it is the thermal overload protection temperature?