Part Number: LM5085
Hi E2E,
I use WEBENCH to design, and choose LM5085 to design.
Vin=56V, VOUT=50V, IOUT=0.5A ; The circuit as below.
When I test short circuit protection (Vout touch GND), The IC is burned out every time.
We find out the VCC pin is damage of burned out IC, the impedance just only 8.8 ohm~200 ohm. (OK IC is 4M~8M)
I try to modify the RADJ to 200R (current limit is 800mA), but IC still be burned out again.
How to modify the circuit to comply SCP?
How to choose D14 IF value?