Hello,
I am planning to build a custom UPS (uninterruptible power supply) with this chip. My questions are:
- Does this typical schematic application in Figure 19 allow for pass through charging? What I mean by that is, when I have the AC adapter attached, will I be sourcing current straight from the adapter, and part of that current will go to charging the batteries if they need charging?
- If I have my AC adapter plugged in, and I have a fully or even half-charged battery attached, when I disconnect the AC adapter, will I see a momentary drop in voltage/current? And, will this drop in voltage/current be significant enough to cause my system to restart (if connected to a MCU)?
- Likewise, if I disconnect my batteries in that same setup as above, will I also see that momentary drop that might cause my system to restart?
- If I use an AC adapter that outputs say 12V/20A, and I set my current limit for charging to 10A on this chip, that means I can still safely charge my batteries at 10A, and then use the other 10A for my system, correct?