Finally the board is working and charging the battery.
the problem now is that charging current is very low, is about 40 to 80 ma.
how I can control the charging current so it at list it will be 500ma to 1A?
Shraga
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Finally the board is working and charging the battery.
the problem now is that charging current is very low, is about 40 to 80 ma.
how I can control the charging current so it at list it will be 500ma to 1A?
Shraga
We did check and it works like the evaluation board
When the battery was low we get around 600ma charge current
We would like to know how we can increase the charge current let's say up to 1.5 A
Thank you in advance
Shraga
5126.SCHEMATIC1 _ PAGE1.pdf5126.SCHEMATIC1 _ PAGE1.pdf
I did check and all the test points the same like in the evaluation board
The input power is from a regular power supply 24V
the battery is a car battery 12v 100 amp
we would like to know how we can control the charging current - increase it up to 2A
Shraga
dear
we have the same problem with TI evaluation board - bq24650EVM
please let me know how we can change the charging current
Shraga
good morning
1. I would like to mention that we are also testing your evaluation board and we get the same value
2. I would like to ask if I can control the charging current?
3. what would be happened if we take OFF the EN_TERM?
thank you in advace
Shraga.
dear Joel
What is the value of RSNS if we would like to charge up to 2A the battery
on the Evaluation board is 0.02
how we can calculate this resistor value?
Shraga
dear Joel8.3.3 Battery Current Regulation
Battery current is sensed by resistor RSR connected between SRP and SRN. The full-scale differential voltage
between SRP and SRN is fixed at 40 mV. Thus, for a 20-mΩ sense resistor, the charging current is 2 A. For
charging current, refer to Equation 3:
The charging current max 640 MA and i cant get 2A like in the datasheet
please let me how to increase to 2A
Shraga.
Dear Joel.
As I said before we did check with TI evaluation board and we get the same results.
Acutely our board is a copy of TI evaluation board so I don’t see how the datasheet said 2 A and we get only 600 ma max.
The power comes from the power supply so we don’t have a current problem
Please let us know what to do how we can increase the charging current and reach at list 1.5A pic
why we can get simple answers about how we can increase the output current?
Shraga