This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92075: How can I increase the PF value and stabilize it ?

Part Number: TPS92075

My circuit requires a power factor (PF) greater than 0.9, so I chose to use the TPS92075.Its architecture is a buck converter.

After referring to the circuit design example, the PF value of my circuit would vary between 0.8 and 0.9. How can I increase the PF value and stabilize it?

The specifications are as following :

Vin=110V AC
Vo=55V DC
Iout=18mA
for LED lighting