Other Parts Discussed in Thread: BQ29200
I now that this integrated circuit is a first level battery protection device and usually it is embedded in the battery protection circuit, but can I use it as a second level protection circuit?
I mean, in my circuit design I want to provide the possibility to use (removable) batteries without built-in protection circuit, so I thought to utilize the BQ29700 in my PCB. Can I do it?
For the batteries that already have a built-in protection circuit, I think it could be seen as a redundancy circuit.
If it is possible, do I have to implement reverse voltage protection diodes?
Another doubt is that for my project I need 2 series cell battery pack (7,4V LiPo), but the BQ29700 IC is suitable only for single cell batteries, so, can I stuck two BQ29700 in series and each protection IC is in parallel with its battery? I attach the block diagram of what I have in mind:
Any suggestion?
Thank you for your attention.