Hello,
We are using the LM5118 Buck boost IC in one of our projects. The switching frequency for the same has been set to 420kHz. We are observing lot of emissions from the particular IC which is resulting in the failure of RE102 test. The emission is observed in 100MHz to 200MHz band and 200MHz to 1GHz frequency bands. The emission level around 130MHz to 180MHz is crossing 50dBuV/m.
We also have a Common mode filter and EMI filter prior to Buck Boost IC.
In one of the article by TI, I read that the Emissions could be reduced by adding a resistance to the High side Mosfet but no where the value of resisitor to be used has been specified.
could anybody please provide an appropriate solution for the same.