This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3817: design of 1.5kw Boost pfc

Part Number: UCC3817

For Design of BOOST PFC

input voltage- 100(min) to 300(max)

frequency- 50Hz

Output voltage- 400 (min)  450(max)

Output Power- 1.5Kw

Switching frequency - 100Khz

 

can be design using UCC3817 PFC ic ?

if not please suggest the suitable Boost PFC for Above mentioned design Parameters

thank you 

regards 

Bharat P. upadhye