Hello,
for a new project at 28-30V, I have the need to measure the current of a line normally closed at the end with a 3,9k Ohm resistor.
I have to monitoring the current flow in these cases:
1) 3,9k Ohm end-of-line
2) 3,9k Ohm || 1kOhm
3) 500 Ohm || 1kOhm
4) 220 Ohm || 1kOhm
5) infinite Ohm (open circuit)
6) <10 Ohm (short circuit).
Normally in the old project I have a shunt resistor of 470 Ohm.
All resistors have 5% of tolerance, but the resistances for resistive dividers (to interface to MCU) have tolerance of 1%.
Now, for a new project I want to try us use TPS2H000 or TPS4H000, because I have 4 and 8 channels.
But my doubt is if the accuracy of current sensing is enough to measure these specific current values or the accuracy is not good for this application?
Thank You in advanced!
Best regards
Federico Battaglin