I'm currently testing a circuit that includes the TPS2511QDGNRQ1 USB Dedicated Charging Port Controller and Current Limiting Power Switch. The documentation says that the values for D+ and D- should be one of the values: 2.0V, 2.7V, or 1.2V. I however am getting values ranging from 0.11V to 0.177V. I was wondering if anyone could shed some light on this? Below is the implementation.